Heating for your home
> Why Floor Heating
> For Renovation
> For New Build
> Outdoor Heating
> Products
> Support and Service
> Documentation
 
 
 
 
SiteLogo
Frost protection of water pipes

Water Pipes

There are two main purposes for using DEVI pipe heating systems:

  • frost protection of pipes
  • maintenance of the required temperature in pipes

Frost protection systems are installed where there is need to prevent water and sanitary pipes from becoming frozen or being damaged by ice.

These systems are especially used in cases where waterpipes are poorly – or perhaps even un-insulated. This can be the case in older houses with waterpipes in walls or on roofs or it can be the case as regards outside pipes which cannot be buried in frost free dept.

Temperature maintenance systems are installed to ensure that hot water or fluid pipes maintain the required temperature.

Inside or outside the pipes

DEVI pipe tracing systems can be installed inside or outside pipes, for indoor and outdoor pipe networks as well as for pipes above and below the ground.

DEVI pipe tracing systems which consist of Deviflex™ heating cables, Devireg™ thermostats and installation accessories.

Devireg™ thermostats with sensors ensure that the absolute minimum amount of energy is used to achieve the optimal result.

Product choise:
Depending on the tube/pipe we recommend:

For outside installation
Deviflex™ electrical heating cables type DTIP-8/10  

For inside installation
Deviflex™ DTIV-9 and DPH-10 (Devi-Pipeheat™)

controlled by an electronic Devireg™ 316, 330 or 610 thermostat which ensures that heat is only switched on when needed.
DEVI Ice and snow melting

Outdoor systems

DEVI’s ice and snow melting systems provide safe traffic during the winter months and safety against damages on buildings and roads during the winter.

DEVI’s systems take care of the problems before they arise and in that way provide security and safety in an environmental balanced way