Heating for your home
> Why Floor Heating
> For Renovation
> For New Build
> Outdoor Heating
> Products
> Support and Service
> Documentation
 
 
 
 
SiteLogo
With a DEVI electrical heating system the service cost are low too compared with all other heating systems

Why an electrical heating system?

An electrical floor heating system has lower installation costs compared with water or air borne heating systems, especially in smaller or energy efficient houses houses. Electricity is always present so the power supply only needs to be scaled where other heating systems needs their own supply, like an oil or gas burner, a district heating unit or a heat pump.

Where most heating systems have an effeciency lower than 100%, electrical heating system are 100% effective. This means that you don't use more energy than required to maintain your house comfortable warm.

Devireg timer thermostats helps you further to save energy without loosing comfort. It is especially relevant for storage heating with low tariff electricity periods or if you want to lower the temperature when you are at work or during night.

Low service cost

With a DEVI electrical heating system the service cost are low too compared with all other heating systems.

Devi heating cables are long-life with guarantee and apart from the relay in the thermostat there are no movable parts like pumps, valves or compressors and is thus maintenance-free.
DEVI quality of life

Heating for your home

DEVI is a Danish company and the world’s largest manufacturer of floor heating systems.

You can confidently install electric floor heating under all types of flooring such as wood, tiles, laminate and linoleum.

With our energy-saving heating system you get cosy comfort and quality of life in your home