Heating for your home
> Why Floor Heating
> For Renovation
> For New Build
> Outdoor Heating
> Products
> Support and Service
> Documentation
 
 
 
 
SiteLogo
Devidry easy floor heating

The world’s best shortcut to floor heating

With Devidry™ it has become even easier to achieve the high levels of comfort that characterise electric floor heating. We call it the Click System, because Devidry™ simply clicks together and does not require the usual layer of filler screed between the heat source and the floor.

Devidry™ consists of soft and bendable materials which are easy to roll out and adapt to the exact measurements of any room. When the floor is covered, it is easy to click the one-metre-wide elements together, and connect the Devidry™ to one of the two thermostat kits of your choice. That is all it takes to install the underfloor heating.

Then you are ready to fit e.g. new wooden flooring and enjoy life with warm feet for the whole family.

Top-quality safety

The patented Devidry™ is the first electric floor heating system in the world which has been certified to the new standard for re-movable floors.

This means that the system has been thoroughly tested and has passed all the strict requirements with flying colours. This means that you as a homeowner can be sure that the system is a quality product.