Heating for your home
> Why Floor Heating
> For Renovation
> For New Build
> Outdoor Heating
> Products
> Support and Service
> Documentation
 
 
 
 
The warm floor keeps the floor’s surface free from slush and water

Utility Room

Utility rooms and halls get so much more from electric underfloor heating than just a pleasantly warm floor.

In these areas, underfloor heating also helps to keep the floor dry. This is particularly useful in the winter when shoes bring wet snow and dirt into the house.

The warm floor keeps the floor’s surface free from slush and water and makes it easier to keep clean. The warm floor also helps to dry wet shoes and boots, making them lovely and warm to put on. In this way, underfloor heating is an effective means of preventing a cold.    

Product Choice

Choose Devireg™ 130/530 or a timer thermostat Devireg™550 or 535 to adjust the temperature to your daily rhythm and in that way save energy. Devireg™ 535 includes a floor sensor which will keep your floor warm regardless of the time of year.
Choose Devilink for an advanced, wiereless, easy-to-understand heating.

When renovating we recommend using Devimat™ DTIF or Devimat™/Deviflex™ DTIR to ensure a low building height when installing floor heating on an existing floor.

For new build where the cables or mats are installed in the concrete slab, we recommend using Deviflex™ DTIP, Deviflex™ DTIE, Devimat™ DTIP or Devimat™ DTIE.