Easy to use – easy to install
The system is very easy to adjust, but if the homeowner does encounter problems, he/she can quickly get back on the right track by just pressing a help button.
“We have put a lot of effort into developing a simple and user-friendly system that is a joy to use. Userfriendliness is also supported by the design, which is minimalistic and with clean lines, without a mass of confusing buttons,” says Devilink™ project manager, Jesper Vraa.
Now, installers can also look forward to getting their hands on the Devilink™ wireless system. It will mean they no longer have to run wires through all the rooms of the house, saving them valuable time as a result.