Electrical Floor Heating
News of current interest
> News Overview
> DEVI News
> Market News
> Press Releases
> News Archive
 
 
 
 
Electrical Floor Heating

Warmth and wellness in your bathroom

04 July 2008

PRESS RELEASE
June 2008
DEVI

Personal care, aromatic relaxation and delightful luxury. Wellness has become a bit of a buzz word recently, and more and more people are dreaming about transforming their bathroom into an oasis of calm and wellness. An electric underfloor heating system from DEVI will put the finishing touches to your dream bathroom in perfect harmony with a spa, shower cubicle and exclusive fittings.

For many people, the bathroom has become the preferred refuge for a time-out for some personal pampering in a busy day. To create the right atmosphere of luxurious wellness, more and more people are fitting out their bathroom with elegant lighting, extravagant tiles and exclusive fittings.

In addition to creating the right mood, most changes are also aimed at making the bathroom visually attractive. But to put the finishing touch to the relaxing refuge, many people are choosing a solution that is hidden under the floor, because without underfloor heating, the dream can quickly evaporate.

Pampering for bare feet

An icy cold floor can quickly spoil the enjoyment of a therapeutic bath and aromatherapy. With the electric underfloor heating system Devimat from DEVI, the self-pampering will begin the moment your bare feet touch the warm floor.

The underfloor heating system from DEVI distributes the heat evenly and pleasantly throughout the entire room. At the same time, a special sensitive thermostat micro-adjusts the temperature, so that the bathroom is always at the right temperature regardless of the time of year.

Quick and easy installation
The ability of underfloor heating to heat the entire bathroom means that in many cases the radiator can be removed altogether. Devimat is ideally suited to refurbishments, regardless of whether you are planning a light face-lift or major rebuilding.

Devimat consists of 3-millimetre cable mats, which can be installed quickly and easily on top of your existing flooring. This eliminates the onerous task of breaking up the old floor and casting in wet cement. Overall, it results in a more effective process and a cheaper installation bill at the end of the day.

No unnecessary energy
In a time with a stronger focus on energy-efficient behaviour, the efficient adjustment of the heat and the placement of the cable mat a few millimetres under the floor mean that no unnecessary energy is used in maintaining a pleasant temperature in the wellness oasis.

With electric underfloor heating, the stage is set for enjoyment and relaxation far away from the stresses and strains of everyday life, without the need to worry about your next electricity bill.