Business and shop centre in Moscow
02 October 2008
New the huge business and shop centre with the hotel - “Metropolis-2” is building in Moscow (Russia).
Total area of “Metropolis-2” is 250000 m2. Also there is a car park on 2000 car places.
There are a lot of branch lines and footsteps which will heat DSOT cable (outdoor installation). It was installed 78400 meters of DSOT and 23 pcs. of Devireg 850.Sum of power is 2350 kW.