Heating for your home
> Homeowner
> Why Floor Heating
> For Renovation
> For New Build
> Snow Melting
> Products
> Support and Service
> Documentation
> Online Thermostat Tutorial
 
 
 
 
 
SiteLogo_en-US
Frost protection of water pipes

Water Pipes

There are two main purposes for using Danfoss pipe heating systems:

  • frost protection of pipes
  • maintenance of the required temperature in pipes

Frost protection systems are installed where there is a need to prevent water and sanitary pipes from becoming frozen or being damaged by ice.

These systems are especially used in cases where water pipes are poorly – or perhaps even un-insulated. This can be the case in older houses with water pipes in walls or on roofs or it can be the case as regards outside pipes which cannot be buried in frost free dept.

Temperature maintenance systems are installed to ensure that hot water or fluid pipes maintain the required temperature.

Inside or outside the pipes

Danfoss pipe tracing systems can be installed inside or outside pipes, for indoor and outdoor pipe networks as well as for pipes above and below the ground.

Danfoss pipe tracing systems which consist of PX pipe tracing cables, PX thermostat and installation accessories. 

Danfoss PX thermostat with sensors ensures that the absolute minimum amount of energy is used to achieve the optimal result.

DEVI Ice and snow melting

Outdoor systems

Danfoss's ice and snow melting systems provide safe traffic during the winter months and safety against damages on buildings and roads during the winter.

The Danfoss systems take care of the problems before they arise and in that way provide security and safety in an environmental balanced way