Precise Control of Danfoss Electric Floor Heating
The Danfoss LX electronic thermostat with floor sensor ensures precise controls of your floor heating system.
The floor will be nice and warm, and never to hot to risk any damages. That way the temperature in the floor construction is always in accordance with the tolerance level that the manufacturer of the floor surface has recommended.
Danfoss is also a favourable option from the point of view of operating costs. Together, the positioning of the source of heat under the floor and the very precise thermostatic control ensure an exceptionally high level of energy utilisation.
Typically, floor heating makes it possible to lower the average room temperature by 2º C without affecting the degree of comfort. This means that the energy loss can be reduced by around 10-20% - which is both an economic and an environmental advantage.