Upcoming Events
> News Overview
> Danfoss News
> Danfoss Events
> Press Release
 
 
 
 
 
SiteLogo_en-US
Danfoss Booth

Danfoss Attending 2009 Construct Canada

01 October 2009
The 2009 Construct Canada Show takes place Dec 2-4 at the Metro Toronto Convention Center in Toronto, ON.

Danfoss will be featuring all of its floor heating and snow melting products as well as introducing the new REVOLUTIONARY Danfoss Reflect Insulation plates. Danfoss Reflect allows the LX floor heating system to be placed under engineered wood or laminate flooring.

The combination of an insulating subfloor and a heat-conducting surface ensures optimum heat reflection upwards. As a result, a relatively low amount of power will suffice to provide the desired heating comfort and reaction time.  The system can be installed on concrete floors or directly on wooden floors without additional preparation. Danfoss Reflect provides the necessary insulation against the subfloor.  

Danfoss will also features its new programmable floor heating thermostat for the LX floor heating system.

Visit  our booth, #820.