Upcoming Events
> News Overview
> Danfoss News
> Danfoss Events
> Press Release
 
 
 
 
 
SiteLogo_en-US
Danfoss Reflect

Danfoss does it again with America’s FIRST Heat Insulation Plates for electrical heating under laminate and engineered wooden floors.

23 September 2009
If your home is in need of a face-lift, the exclusive dream of a warm wooden floor could soon become your reality. With Danfoss’s revolutionary new product, Danfoss Reflect, installing a warm wooden laminate floor is quick, easy and sure to please the whole family.  

More and more homeowners are giving their homes a face-lift to create their ideal home. If your home needs modernizing, under floor heating under a wooden laminate floor is the perfect solution for creating a warm-hearted home. This is because Danfoss Reflect keeps the whole family warm from head to toe.
 
Under floor heating under a laminate wooden floor Under floor heating is no longer limited to stone or tile. Danfoss Reflect can be installed under a wooden laminate floor in just about any location in the home. The natural look and feel of the wood is not affected by the underlying insulating sheets or the rising heat because the heat is given off in a gentle and controlled manner.  

Making it easy for the professionals The difficult task of laying, levelling and setting cement and other materials often took professionals several days. Now you simply lay the insulating heat distribution plates on the existing floor, press the heating cable into place, lay the wooden floor directly on top, connect the thermostat, and you can turn on the heat!  It cannot get any simpler, faster or cleaner… 

The combination of an insulating subfloor and a heat-conducting surface ensures optimum heat reflection upwards. As a result, a relatively low amount of power will suffice to provide the desired heating comfort and reaction time.  The system can be installed on concrete floors or directly on wooden floors without additional preparation. Danfoss Reflect provides the necessary insulation against the subfloor.  

Danfoss Reflect consists of a ½” polystyrene plate covered with a 1/32” aluminium plate with a special profile. Depending on the desired effect, the heating cable is installed in each, every second or every third cable groove.
 
The Danfoss Reflect plates are simply and quickly adjusted to curves and angles by using a jigsaw and ensures a good heat distribution even into the border areas of the room.  

Danfoss Reflect is available from your local electrical supplier