Products and technical information
> Products
> Danfoss Solutions
> Construction Project
> Support and Service
> Documentation
> Installer Program
> Online Thermostat Tutorial
 
 
 
 
 
SiteLogo_en-US
Best warranty in the industry

Actually the best warranty in the market.

A floor heating system which does not works causes not only dissatisfied customers - it also causes angry customers and with good reason.

A heating cable which is not working is not so easy to replace. The fault has to be found the floor must be taken up before the fault can be corrected. It is a difficult, dirty and expensive process.

Therefore Danfoss find it of great importance to produce in extremely high quality - also if it means that the price can be higher than other products. In return we offer the market's highest security for unproblematic function. And we back up the promise with the best warranty in the market.

In the event of a fault that can be traced back to a manufacturing defect in a Danfoss LX, GX, or TX heating mats or cables Danfoss will cover the cost of the product itself, along with any damage to bricklaying and tiles, for example, at no extra cost to the customer.     

Danfoss meets the warranty conditions

Naturally, Danfoss meets the warranty conditions specified in national sale of goods acts and in the EU’s own Sale of Goods Act.

We therefore provide:

  • 2 year warranty for thermostats and controls
  • 2 year warranty for RX roof and gutter and PX pipe tracing heating cables
  • Genuine 10 year non-prorated warranty for all LX, GX, and TX heating mats and cables.