Welcome to DEVI

  • Overview
  • Electric heating applications
  • Products
  • Warranty
  • Tools and apps
  • News
  • Articles
  • Case stories
  • Learning
  • Contact us

Make it easy, Make it DEVI

DEVI is a Danfoss Group subsidiary and a global leader in heating. With a focus on quality and durability, we continue to leverage decades of experience to produce quality products, ranging from electric underfloor systems to outdoor heating solutions.

Read more about our applications
Building

Electric Heating solutions for indoor comfort and outdoor safety

As the global supplier of electric indoor and outdoor heating solutions, we master advanced, heat-control technology that optimizes user comfort, safety and energy savings.

Why electric heating?

Electric heating wind

Electric heating a good answer to rising energy costs

As the world faces rising gas prices and supply uncertainty, electric heating powered by electricity from renewable energy sources is gaining importance as a valuable and sustainable heating option.

Indeed, demand for electricity is forecast to grow to 30% in 2030 and to reach 50% by 2050 as we make the transition to climate neutrality. By 2050, the European Commission is aiming for 84 percent of this demand to come from renewable energy sources which will significantly decrease CO2 emissions. 

When combined with modern, intelligent controls electric heating can make grids smarter and facilitate renewable energy consumption. And moreover, with the use of electric heating, no harmful substances are emitted to the air or to the soil.

Electric underfloor heating is a major opportunity for Europe. This can play a significant role in helping Europe reduce emissions, increase energy efficiency in buildings, and ultimately enable Europe to meet its ambitious climate targets. 

heating energy

Electric heating is cost efficient solution

Electric underfloor heating in combination with solar PV is perceived for the most cost-efficient heating solution when it comes to highly insulated residential buildings. Electric underfloor heating is also set to become cheaper for consumers than traditional gas, liquid and solid fuel technology.

Electric heating enables a comfortable room temperature with the lowest possible energy consumption. Room temperature can be reduced by 1 - 2 °C on average compared to traditional radiator heating, saving energy use and costs. 99% of the energy consumed by the electric underfloor heating is converted into heat, thus maximizing its energy efficiency and avoiding unnecessary energy losses by having to circulate water, for example. 

electric heating meter

Why is electric heating energy efficient?

An electric heating system achieves the required temperature quickly depending on the floor construction, so rooms can be heated only when required for amazing energy savings. Together, the positioning of the source of heat under the floor and very precise thermostatic control ensure an exceptionally high level of energy utilization efficiency, for reduced energy consumption without compromising thermal comfort.

Benefits of electric underfloor heating

A comfortable ambient temperature and quick response time are just a couple of the benefits electric heating offers. Learn more about these and other benefits of electric heating.

Electric heating applications

DEVI

Products

  • if (isSmallPicture) { Digital Thermostats; } else if (isBigColumns) { Digital Thermostats } else { Digital Thermostats }
    Digital Thermostats

    Digital controllers have the unique features allowing you to reduce energy waste. Some thermostats are fitted with Wi-Fi allowing remote control of heating systems via mobile application.

  • if (isSmallPicture) { ; } else if (isBigColumns) { } else { }
    Indoor Thermostats

    The indoor thermostat is an integral component of the electric heating system, used to control the floor heating.
    Thermostats are electronic devices allowing precise control of the floor surface or air temperatures. They are equipped with air or/and underfloor temperature sensors control the heating element.

  • if (isSmallPicture) { Heating mats; } else if (isBigColumns) { Heating mats } else { Heating mats }
    Heating Mats

    The heating mats are used for installation in a thin layer of tile adhesive, self-leveling mixture, or similar. The standard minimum thickness of the floor layer is 5-8 mm while the thickness of electric heating mat is 3–4.5 mm. This minimizes the floor level increase. Electric heating mats consist of a thin cable securely fixed on self-adhesive glass-fiber mesh, usually of 50 cm width. Thin heating mats are manufactured as ready-made heating sections with a specific area (i.e. 0.5, 1, 1.5 … 12 m²) including a power supply cable (cold lead) and hermetically sealed connections.

  • if (isSmallPicture) { Heating Cables; } else if (isBigColumns) { Heating Cables } else { Heating Cables }
    Heating Cables

    Heating cables are used for a variety of applications, including indoor comfort floor heating and total heating both for small houses as well as large commercial buildings.
    Heating cables are mostly used in connection with new building or larger renovation projects.

     

Warranty

Devi

Warranty

DEVI has consistently delivered value to customers through a commitment to quality, reliability, and innovation. Our products are supported by industry-leading assistance including the DEVIwarranty™.

It not only covers the replacement of cables or mats but also extends to the reimbursement of installation and material costs for up to 20 years!

Comprising five individual warranties, DEVI provides you with complete peace of mind when using Electric Heating products.

Tools and apps

News

  • if (isSmallPicture) { 80 years of DEVI / Electric heating; } else if (isBigColumns) { 80 years of DEVI / Electric heating } else { 80 years of DEVI / Electric heating }
    80 years of energy efficient and environmentally friendly electric heating innovation
    Monday, June 27, 2022

    DEVI Electric Heating is creating more comfortable indoor environments with floor heating applications in bathrooms, kitchens, bedrooms, offices, infact anywhere where warmth is required. In addition to these indoor solutions, DEVI's electric heating cable technology is also widely used in outdoor applications, ensuring safety in winter period by minimizing the hazards of snow, frost and ice or their consequences.

  • if (isSmallPicture) { Electric heating on the rise; } else if (isBigColumns) { Electric heating on the rise } else { Electric heating on the rise }
    Welcome to the new home of DEVI
    Monday, June 27, 2022

    Welcome to the new home of DEVI
    DEVI and Danfoss electric heating are now in one place. We’re bringing all our DEVI and Danfoss electric heating content together to our Danfoss website.

  • if (isSmallPicture) { Vineyards frost protection; } else if (isBigColumns) { Vineyards frost protection } else { Vineyards frost protection }
    Vineyards frost protection
    Tuesday, May 24, 2022

    Electric Heating solves the challenge with energy efficient systems using Electric Heating cables to protect grapes against frost damage. Vineyard Frost Protection by Danfoss is a sustainable solution for a green and clean future through low energy consumption during the frost period allowing to safe up to 87% of harvest. Vineyard frost protection by Danfoss is an ideal solution for any vineyard dimension.

Articles

DOs and DON’Ts for Indoor Electric Heating

DOs and DON’Ts for Indoor Electric Heating

Electric Heating is an energy-efficient and environmentally friendly floor heating solution. You can use it for either newly constructed or renovated homes.

Case stories

  • if (isSmallPicture) { ; } else if (isBigColumns) { } else { }
    Electric heating by DEVI provides energy-efficient heating solution for near-zero energy housing complex

    For decades, many have considered electricity to be an inefficient heating source, associating it with high energy bills and pollution. However, times are changing. Now, the combination of electric floor heating and solar panels are an energy-efficient option for homeowners. Yes, the future is indeed electric, as this case from Koblenz, Germany shows.

  • if (isSmallPicture) { The Bjørvika Tunnel, Oslo, Norway; } else if (isBigColumns) { The Bjørvika Tunnel, Oslo, Norway } else { The Bjørvika Tunnel, Oslo, Norway }
    The Bjørvika Tunnel, Oslo, Norway

    Electric heating for the immersed tunnel in Norway.

    The Bjørvika Tunnel is a motorway immersed on European Route E18 in the city center of Oslo. The tunnel links Festning tunnel in Oslo west with Ekeberg tunnel in Oslo east. The completed tunnel has an unbroken length of six kilometers. The Bjørvika Tunnel is the first immersed tunnel in Norway.

  • if (isSmallPicture) { Electric heating system to prevent the condensation in the Woolworths Distribution Centre; } else if (isBigColumns) { Electric heating system to prevent the condensation in the Woolworths Distribution Centre } else { Electric heating system to prevent the condensation in the Woolworths Distribution Centre }
    Electric heating system to prevent the condensation in the Woolworths Distribution Centre

    The Woolworths Distribution Centre was experiencing condensation due to the temperature differences between the cold storage facility and their offices. This resulted in water dripping hazards in the meeting rooms, canteen, and offices.

  • if (isSmallPicture) { Pipe tracing in 600 Suzhou apartments China; } else if (isBigColumns) { Pipe tracing in 600 Suzhou apartments China } else { Pipe tracing in 600 Suzhou apartments China }
    Pipe tracing in 600 Suzhou apartments China

    Suzhou city was founded in 500 BC. is nowadays a major city located in the south-eastern Jiangsu Province of East China, about 100 km (62 mi) northwest of Shanghai. It is a big economic center and local point of trade and commerce, and the second largest city in the province, after its capital Nanjing.

  • if (isSmallPicture) { The Örebro Castle; } else if (isBigColumns) { The Örebro Castle } else { The Örebro Castle }
    Electric heating systems for the conservation of old castles

    The Örebro Castle is a medieval castle fortification situated in the scenic region of Närke, Sweden. The castle lies on an island by the river Svartån. The oldest part of the castle, a defense tower, was erected in the latter half of the 13th century, but its present appearance, the Örebro Castle, was constructed over the last century. Since 1935, the castle has been a national Swedish monument.

  • if (isSmallPicture) { Supporting constant temperature at Montague Apple Orchard and Warehouse in Victoria Australia; } else if (isBigColumns) { Supporting constant temperature at Montague Apple Orchard and Warehouse in Victoria Australia } else { Supporting constant temperature at Montague Apple Orchard and Warehouse in Victoria Australia }
    Supporting constant temperature at Montague Apple Orchard and Warehouse in Victoria Australia

    Montague Apple Orchard, established in 1948, is a key player in the Australian food manufacturing industry with a 70-year legacy.

    In their upcoming Narre Warren Cold Storage Warehouse, a constant temperature of 1°C is required to avoid condensation.

Learning

DEVI

Visit our Learning Center

Danfoss offers online training materials for technicians and designers working with electric heating. All e-lessons are available free and on-demand through Danfoss Learning portal. For more information, register in our support section by following the link or find the overview of available relevant trainings in the table below.

Contact us

For further information, please contact us for technical support