Products and technical information
> Products
> DEVI Solutions
> Construction Project
> Project References
> Support and Service
> Documentation
 
 
 
 
SiteLogo
Interaction with the building process

Interaction with the rest of the building process

There is more to efficient building than just the ease and speed of the installation of a specific product alone. Actually the way a certain product and installation process fits into the rest of the building procedure is sometimes even more important.

The installation of a DEVI floor heating system fits perfectly into the building process with an efficient two step process.

Step one: As soon as the rough building is ready, heating cables or mats are attached to the basic floor and the system is typically covered with a thin layer of self levelling cast concrete. The thin layer of concrete means a very short hardening time: after just one day of hardening (skal bekæftes) you can set foot on the floor making space for the next team of craftsmen.

Step two: The heating cables or mats are connected to the thermostat and again to the buildings power supply in continuation of the electrician’s final connection of the buildings other supply.

DEVI has experience

DEVI has a large documented experience with large building projects and considerable expertise in integrating the installation of its products in the entire building project.
Intelligent heating

Intelligent heating systems

DEVI is a Danish company and the world’s largest manufacturer of floor heating systems.

In our centre of competences we constantly develop energy-saving heating systems.

With our heating system you get security and guarantee for quality.