Frost protection of tank systems
Tanks placed in open or cooled areas as e.g. in the food industry might pose a problem when they carry temperature dependent liquids as e.g. broth.
If the tanks are cooled under a certain temperature, the liquid will coagulate in the tank and in the pipes.
In such cases it is necessary to maintain a preset temperature in the tank plant. This is done by winding pipes and tanks with Deviflex™ heating cables.