Evinizi Isıtalım
> Consumer
> Neden Elektrikli Döşemeden Isıtma
> Yenilenen Binalarda
> Yeni Binalarda
> Kar-Buz Birikimini Engelleme
> Ürünler
> Destek ve Servis
> Kullanım Klavuzları
 
 
 
 
SiteLogo

Evinizdeki her oda için

Isıtmak istediğiniz alan büyük ya da küçük olsun,DEVI Elektrikle Döşemeden Isıtma Sistemi her türlü alanlar için uygun çözümler sunar.

DEVI Elektrikli Döşeme Sistemi düşünebildiğiniz her yüzeye uygulanabilir.

DEVI Elektrikle Döşemeden Isıtma Sistemi görünmezdir ve evinizin dekorasyonunda size özgürlük sunar.Çünkü yer kaplayan ve boşluklar oluşmasına neden olan borular ve radyatörler bulunmaz.

Banyo 

Özel dizayn edilebilecek durumda ve yerden ısıtılma konforunun yaşandığı bir banyoyu hayal edebiliyor musunuz? Akıllı ısıtma sistemlerine sahip Devi ile bütçenizi sarsmadan böyle bir banyoya sahip olabilirsiniz. 

Elektrikli döşemeden ısıtma sistemi ile radyatör ve borulardan kurtularak banyonuzu rahatça dizayn edebilirsiniz.
 

>Daha fazla

Kitchen

Do you dream of a nice and inviting kithchen? Most families spend a lot of their time in the kitchen and therefore flooring is very important for the familiy's well-being. 

Underfloor heating is very well suited for kitchen floors, because it supplies a nice warmth discreetly hidden under the floor.

It leaves the room to be designed as you wish without having to consider the placement of radiators and visible pipes.

>Daha fazla

Living room

The living room is intended for rest and relaxation
The living room is for relaxing after a busy day. Perhaps together with family and friends. Perhaps in solitude with a good book or an interesting television programme. Perhaps you enjoy playing on the floor with your children. All these activities make demands on your heating system.

Underfloor heating is always near at hand
When you want to relax, the heating system in your living room will ensure a comfortable temperature that is neither too cold nor too warm. Above all, heat must be supplied to the room being used by the family.

In the living room, you sit still and are close to the floor, which is why a DEVI underfloor heating system is ideal. This ensures a pleasant warmth at floor level and a comfortable temperature at sitting level.  
>Daha fazla

Playroom and bedroom

A child’s room is a room for having fun in, where children can play on the floor, read exciting books and enjoy a good sleep. Such rooms do, however, have some unique heating requirements.

On the one hand, a child’s room must be pleasantly warm throughout the day to make it suitably inviting. On the other hand, it must be cool enough in the evening and during the night to encourage a good, deep sleep.

DEVI’s advanced heating systems make it easy to control and optimise the temperature in children’s rooms.
>Daha fazla