Welcome to DEVI

Make it easy, Make it DEVI

DEVI is a Danfoss Group subsidiary and a global leader in heating. With a focus on quality and durability, we continue to leverage decades of experience to produce quality products, ranging from electric underfloor systems to outdoor heating solutions.

Building

Electric Heating solutions for indoor comfort and outdoor safety

As the global supplier of electric indoor and outdoor heating solutions, we master advanced, heat-control technology that optimizes user comfort, safety and energy savings.

Why electric heating?

Electric heating wind

Electric heating a good answer to rising energy costs

As the world faces rising gas prices and supply uncertainty, electric heating powered by electricity from renewable energy sources is gaining importance as a valuable and sustainable heating option.

Indeed, demand for electricity is forecast to grow to 30% in 2030 and to reach 50% by 2050 as we make the transition to climate neutrality. By 2050, the European Commission is aiming for 84 percent of this demand to come from renewable energy sources which will significantly decrease CO2 emissions. 

When combined with modern, intelligent controls electric heating can make grids smarter and facilitate renewable energy consumption. And moreover, with the use of electric heating, no harmful substances are emitted to the air or to the soil.

Electric underfloor heating is a major opportunity for Europe. This can play a significant role in helping Europe reduce emissions, increase energy efficiency in buildings, and ultimately enable Europe to meet its ambitious climate targets. 

heating energy

Electric heating is cost efficient solution

Electric underfloor heating in combination with solar PV is perceived for the most cost-efficient heating solution when it comes to highly insulated residential buildings. Electric underfloor heating is also set to become cheaper for consumers than traditional gas, liquid and solid fuel technology.

Electric heating enables a comfortable room temperature with the lowest possible energy consumption. Room temperature can be reduced by 1 - 2 °C on average compared to traditional radiator heating, saving energy use and costs. 99% of the energy consumed by the electric underfloor heating is converted into heat, thus maximizing its energy efficiency and avoiding unnecessary energy losses by having to circulate water, for example. 

electric heating meter

Why is electric heating energy efficient?

An electric heating system achieves the required temperature quickly depending on the floor construction, so rooms can be heated only when required for amazing energy savings. Together, the positioning of the source of heat under the floor and very precise thermostatic control ensure an exceptionally high level of energy utilization efficiency, for reduced energy consumption without compromising thermal comfort.

Benefits of electric underfloor heating

A comfortable ambient temperature and quick response time are just a couple of the benefits electric heating offers. Learn more about these and other benefits of electric heating.

Electric heating applications

DEVI

Products

Warranty

Devi

Warranty

DEVI has consistently delivered value to customers through a commitment to quality, reliability, and innovation. Our products are supported by industry-leading assistance including the DEVIwarranty™.

It not only covers the replacement of cables or mats but also extends to the reimbursement of installation and material costs for up to 20 years!

Comprising five individual warranties, DEVI provides you with complete peace of mind when using Electric Heating products.

Tools and apps

News

Coming soon...

Coming soon...

Articles

DOs and DON’Ts for Indoor Electric Heating

DOs and DON’Ts for Indoor Electric Heating

Electric Heating is an energy-efficient and environmentally friendly floor heating solution. You can use it for either newly constructed or renovated homes.

Case stories

Learning

DEVI

Visit our Learning Center

Danfoss offers online training materials for technicians and designers working with electric heating. All e-lessons are available free and on-demand through Danfoss Learning portal. For more information, register in our support section by following the link or find the overview of available relevant trainings in the table below.

Contact us

For further information, please contact us for technical support