Sun Village, Byala Black sea region

SUN Village Byala is a holiday complex with 18 houses. The beach of Byala with fine white sand, clean water is just 300 meter away the village. The SUN Village Byala is the only resort of its kind on the Bulgarian Black Sea coast. In 2007 the resort won an architectural award as the year's best project in the Varna region.

Also in 2007 DEVI floor heating systems installations for bathrooms and main rooms in 16 houses of the Sun Village was completed.

Project Overview:

Electrical floor heating

Project size: 16 houses  

Total output:     52 kW

Products:

DEVIflex™ DTIP 18

DEVIreg™ 530, 535

[Project Size]

16 houses

Нагревателни кабели
Терморегулатори