Full range of electric heating, private house, Ukraine
This Ukrainian house is an excellent example of using DEVI electrical heating solutions for heating and winter protection by a private owner. Almost all DEVI electrical heating solutions were implemented in the one building, from floor heating to pipe tracing to the ice and snow melting system on the roof and ground.
Project Overview:
Three snow melt systems on the open area
Comfort heating - 18 systems
Two-story building complete, heating garage wall convectors
Frost protection of a small section of the pipeline
The heating system on the roofs of two separate buildings
Products:
DEVIflex™ DTIP-18, DSIG-20, DTCE-30, DTIP-10,
DEVImat™ DTIR-150
DEVIreg™ 530; 550; 330; 850
Gallery
[Project Size]
NA
Topné kabely
Topné rohože
Regulační prvky