Saint Catherine’s Church Gdansk, Poland
St Catherine's Church is the oldest church in Gdańsk. Primarily, it was a Protestant church from 1545 to 1945, when it became a Roman Catholic Church. It is worth mentioning that the first pulsar clock in the world is also there.
Project Overview:
Ice & snow melting system for drains and channels on the roof.
Project size: 170 m2
Products:
DEVIsnow™ 30T
DEVIreg™ 850 + gutter’s sensors – 4 pcs
Gallery
[Project Size]
170 m2
Topné kabely
Regulacní prvky