The Grid, Rushcutters Bay, Sydney, Australia
The Grid is a seven-story apartment building containing 38 units and 2 underground parking levels for 44 cars. DEVI was chosen to provide the main heating system for all apartments. Construction was completed in 2001.
Since all floors were to be tiled, the system was designed to supply the everyday heating requirements of the occupants. The floor heating was designed so that it would work in conjunction with the air conditioning as a supplementary heat source, if required. Due to building codes, all heating was installed over soundproofing.
Project Overview:
Project size: 38 apartments, a total load of 260kW
Products:
- DEVIflex™
- DEVIreg™ 330
[Project Size]
38 apartments
Topné kabely
Regulacní prvky