New wedding place
Poročna dvorana na Poljskem
asnkasehisnkjsiwjs
There are historic buildings, like palaces, churches, and architectural complexes, of which many actually were destroyed during the War, but reconstructed with great care in the 2nd half of the 20th century; among these, you can find the Wedding Palace – the main venue to get married in Warsaw.
Warsaw’s Old Town and the Wedding Palace were rebuilt after the Word War II using the preserved images and paintings made by the Italian artist, Bernardo Bellotto, called Caneletto, in the 17th century.
Despite the fame of the Wedding Palace, few realize that, since 2007, this building has been equipped with DEVImat™ under 600 m2 of wooden and stone floors. Thanks to DEVI intelligent solutions, all newlyweds and their guests can feel comfortable during the ceremony, no matter how cold it is outside.
We believe that all marriages concluded in the Warsaw Wedding Palace are forever and we wish all the newlyweds all the best!
Project Overview:
- DEVImat™ DTIF-150 on 600 m2
- DEVIreg™
- Capacity - 39 kW
600 m2