Hotels & Commercial buildings

Reasons to install DEVI electrical heating solutions for large public buildings

During its history, DEVI was chosen as the preferred supplier of electric heating for large public buildings, such as shopping malls, hotels, office buildings, and airports all over the world.

You don’t need to heat a whole volume of air in a 15 m high lobby, to be able to assure optimal thermal comfort for visitors (at 2 m height from flor level). Floor heating, ice & snow melting, pipe tracing and other applications are the core of electrical heating solutions offered by DEVI.

1. Experience with large construction

DEVI has proven co-operation with well-known shopping malls, hotels, offices, and other public buildings. DEVI is represented in over 66 countries and you can find public properties equipped with DEVI reliable solutions all over the world. Local DEVI sales companies provide large constructors with professional support and technical help to make our co-operation easy and efficient. 

2. DEVI provides safety

Our solutions are chosen mainly to provide safety for driveways, walkways, roofs, and gutters as well as pipe tracing. DEVI’s ice and snow melting system is designed to provide safety for people, vehicles, and buildings through safe walking and driving, and less damage to buildings during winter.  

Each centralized water system for public buildings, such as hospitals, hotels or multifamily blocks, should be protected against Legionella, not only via efficient filtration and disinfection but also by keeping water temperature within the control limits in the legionellosis risk. DEVI heating systems for domestic hot water meet demands of all required certificates for such pipe tracing.

3. Economical advantages

The DEVIreg™ thermostats with advanced moisture sensors (for outdoor systems) or opened window detectors (for indoor heating) ensure that optimal results are achieved with the least possible amount of energy.

It’s worth emphasizing that the costs of installing and running DEVI’s outdoor systems are low when the preventive advantages of the system are taken into consideration.  You will easily avoid yearly investments in snow shovelling and salting. Furthermore, you avoid the repair costs caused by ice, snow, and salt damage.

DEVI has been chosen as the electric heating partner for buildings as hotels, shopping moles or rest homes, all over the world, mostly for budget reasons.

4. DEVI provides comfort

Floor heating is the most comfortable experience for guests of your hotel rooms or apartments. It distributes the heat evenly over the whole floor and provides appropriately pleasant warmth for your feet, body, and head. The wholesome heat surrounding your feet slowly rises and nicely warms your body. Underfloor heating makes it possible to lower the average room temperature by 2º C without affecting the degree of comfort. This means that the temperature can be reduced by around 20% - which is both an economic and an environmental advantage

5. Up to 20-year full warranty for DEVI cables and mats

All DEVI products are manufactured in the EU under the highest quality control. That’s why you can rely on DEVI.  Due to the quality provided, we offer the best 20-year full warranty for DEVI heating elements, which includes costs of installation and floor materials, such as damage to brickwork and tiles.

DEVI - the reliable partner for large contractors
DEVI is represented in over 33 countries. As the leading manufacturer of electrical heating systems, DEVI has the biggest team of floor heating specialists in the business.
DEVI heating for roofs, gutters and down pipes
DEVI provides a high-tech heating solution to efficiently fight against ice and snow. DEVI ice and snow melting system for roofs consists of heating cables, an electronic thermostat, and installation accessories.
Types of underfloor heating
DEVI floor heating makes the floor comfortably warm and can be installed in all types of floors and with all kind of floor coverings.
Safe, quality and reliable electrical heating
DEVI heating solutions are permitted for use in houses, apartments, and other facilities. Safety is ensured by the high quality, reliable construction of the cables and installation in accordance to building standards.
Why outdoor heating?
Many homeowners experience the challenges of ice and snow with roofs, gutters, downpipes and on the driveway.
DEVI for your roof
DEVI outdoor heating cables are installed to prevent ice and snow from accumulating on your roof. They melt snow, eliminating heavy snow and ice accumulation on the roof. Heating cables stops ice dams from forming on roof edges
DEVI for your gutters
DEVI offers the best solution to avoid ice-related damage to gutters. By running DEVI electric heating cables inside the gutters and downspouts, you can be sure that your gutter will remain undamaged throughout the winter.
DEVI for your driveways and walkways
DEVI offers a modern solution to avoid such hard work, saving your time and money. With DEVI heating cables under your driveway and walkway, you don’t need be weighed down with cleaning snow off your driveway and walkway any longer.
Advantages of electrical floor heating
DEVI electrical floor heating is mounted directly in the tile glue and it only needs 4.5 mm layer under panels. It makes installations easier and faster – you don’t need to waste your time for waiting for few centimeters layer to dry.
5 reasons to install outdoor heating system
DEVI offers a smart and simple solution to keep our houses dry and safe during the winter season. Outdoor heating systems help to save time and money while avoiding unnecessary work.
DEVI 75 – Celebrate with us!
2017 is a historic year for DEVI as it marks our 75th anniversary of providing high-quality heating solutions to many homes and businesses around the world. As part of the celebrations, we are inviting DEVI installers to take part in a special competition.
Great pictures received during the Facebook competition for DEVI 75 years
In the nine-weeks long celebration a lot of customers decided to celebrate together with us. We have received 73 photos from all over the world. Thanks to everyone who has participated in our 75th anniversary celebration!
Happy Holiday Season
We wish you a very Happy Holiday season and a peaceful and prosperous New Year.
DEVI Ice and Snow melting system: installation for a family house
DEVI offers a smart and simple solution to keep our houses dry and safe during the winter season. Outdoor heating systems help to save time and money while avoiding unnecessary work. DEVI ice and snow melting systems consist of electrical heating cables or mats, thermostats, and sensors as well as accessories for installation. Each solution is fitted to meet home owners’ individual needs.