Industrial

Industrial 

Considering that large amounts of sensitive substances are stored in huge tanks, it is crucial to maintain the required temperature of such reservoirs all year long, regardless of the weather conditions. The most flexible and efficient solution for tanks are DEVI electrical heating cables. 

We have been offering heating systems for safety of the industry and pipes security. Frost protection systems may be used for various pipes, tanks and containers within the agricultural and industrial sectors, such as gas, oil, or fire-water tanks.

It may be necessary to protect pipes and tanks against frost and temperature decreasing below the demanded level, to ensure a free passage of materials. It is also important to maintain a certain minimum temperature in tank systems to avoid problems with stiff scraps, coagulation, or frost damage in the tank.

If there is a need to maintain a certain temperature, the heat loss through the insulation has to be compensated to avoid any risk caused by low temperatures or ice, even if the tank is insulated. This may be done by attaching DEVI heating cables to the pipes and tanks.