For any room in your home
Irrespective of whether your heating requirements are large or small, DEVI electrical floor heating ensures efficient, comfortable heating without compromising on interior design. You can find a DEVI floor heating solution suitable and optimized for every purpose imaginable. You can easy equip every room in your house or flat, not only a bathroom or a kitchen, but also a living room, a playroom, and bedrooms as well as a hallway.
The DEVI system is invisible, which gives you new possibilities for furnishing and interior design without having to consider space consuming radiators.
Bathroom
Do you dream about an exclusive bathroom with room for both comfort and style? With DEVI's intelligent heating system you can get you dream fulfilled without putting your finances under pressure.
With an electric floor heating system, you can remove radiators and visible pipes, therefore you can furnish your bathroom as you like; this gives you exciting possibilities to design a completely new bathroom and allows for extra space, especially in smaller bathrooms. DEVI floor heating system completes the sense of comfort.
Floor heating provides comfort in the bathroom
Spa baths, aromatherapy, and relaxation are synonyms of exclusive comfort, but nowadays you can afford to have it on your own. More and more people have acquired a taste for comfort, transforming their bathroom into a modern oasis of wellness.
Elegant lighting, exclusive fittings, and designer tiles alone do not create the atmosphere of comfort. Enjoyment starts with a warm and cosy indoor climate; ice-cold floors must be avoided. In many cases, this means that the radiator is pensioned off to make way for DEVI’s modern floor heating system, which distributes the heating evenly and comfortably throughout the room. At the same time, the system's quick reaction time means that the room will always have an ideal temperature.
<Product Choice for bathroom floor heating:
DEVIreg™ 130/530 or a timer thermostat DEVIreg™550 or 535 to adjust the temperature to your daily rhythm and in that way save energy. DEVIreg™ 535 includes a floor sensor which will keep your floor warm, regardless of the time of year.
DEVIlink for heating that is advanced, wireless, and easy to understand.
When renovating we recommend using thin DEVImat™ DTIF or DEVImat™/DEVIflex™ DTIR to ensure a low height when installing floor heating on an existing floor.
For a new build, where the cables or mats are installed in the concrete slab, we recommend using DEVIflex™ DTIP, DEVIflex™ DTIE, DEVImat™ DTIP or DEVImat™ DTIE.
Kitchen
Do you dream of a nice and inviting kitchen? Most families spend a lot of time in the kitchen; therefore, flooring is very important for the family’s well-being. Underfloor heating is well suited for kitchen floors because it supplies good warmth while discreetly hidden under the floor. It leaves the room to be designed as you wish without having to consider the placement of radiators and visible pipes.
Your kitchen is the center of the home
The kitchen floor has to stand for a little of everything. The kitchen is where the food is cooked;it is here you gather with your family and friends, and your children play on the floor. Ceramic tile is often the primary choice for a kitchen floor. The only disadvantage is that the floor feels cold. However, with DEVI's heating cables or mats, you can turn the cold feeling into a pleasant feeling.
Design your kitchen your way
With the modern heating system hidden away in the floor, you are spared both radiators and visible pipes. This gives you exciting possibilities to design a completely new kitchen and allows for extra space. You don't have to choose between kitchen cabinets or radiators, but can focus on designing the kitchen of your dreams.
Living room
The living room is intended for rest and relaxation after a busy day; perhaps, together with family and friends, in solitude with a good book or an interesting television program, or you enjoy playing on the floor with your children. All these activities make demands on your heating system.
Underfloor heating is always near at hand
When you want to relax, the heating system in your living room will ensure a comfortable temperature that is neither too cold nor too warm. Above all, heat must be supplied to the room being used by the family.
In the living room, you sit still, and close to the floor, which is why a DEVI underfloor heating system is ideal. This ensures a pleasant warmth at floor level and a comfortable temperature at sitting level.
Design and furnish your living room as you please
In the living room, we make your furnishing and design dreams a reality. Here, there are often large glass panels from floor to ceiling that provide an impressive source of light and an incredible view. With an underfloor heating system, you can do away with radiators and visible pipes in front of your windows. Instead, you have an excellent opportunity to design and furnish your living room exactly as you wish.
Common floor coverings in the living room are wood flooring or carpet; both of these work brilliantly with DEVI underfloor heating, as our accurate thermostats can limit the floor temperature to a preset maximum temperature.
DEVI underfloor heating systems are so flexible that they automatically switch off, if a wood-burning stove is lit in the living room on a cold day.
Playroom and bedroom
A child’s room is a room for having fun, where children can play on the floor, read exciting books, and enjoy a good sleep. However, such rooms have some unique heating requirements. On the one hand, a child’s room must be pleasantly warm throughout the day to make it suitably inviting. On the other hand, it must be cool enough in the evening and during the night to encourage a good, deep sleep.
DEVI reliable solutions make it easy to control and optimize the temperature in children’s rooms.
Warm during the day, cooler at night
A child’s room must be warm during the day but cooler at night. This requires a heating system that can be set precisely to suit a family’s living habits. DEVI advanced timer control system and quick-acting underfloor heating system are easily able to meet demands for flexible heating in children’s rooms. An extra benefit is that it is ideal for the heating to be in the floor, as this is a child’s preferred play area when indoors.
It also means parents no longer need to worry about little fingers coming into contact with hot radiators.
Product Choice for playrooms and bedrooms
DEVIreg™ 550/530 to adjust the temperature to your daily rhythm and, in that way, save energy while improving comfort.
DEVIlink for heating that is advanced, wireless, and easy to understand.
When renovating, we recommend using DEVImat™ DTIF or DEVImat™/DEVIflex™ DTIR to ensure a low height when installing floor heating on an existing floor.
For a new build, where the cables or mats are installed in the concrete slab, we recommend using DEVIflex™ DTIP, DEVIflex™ DTIE, DEVImat™ DTIP or DEVImat™ DTIE.
Utility Room
Utility rooms and halls get so much more from electric underfloor heating than just a pleasantly warm floor.
In these areas, underfloor heating also helps to keep the floor dry. This is particularly useful in the winter when shoes bring wet snow and dirt into the house.
The warm floor keeps the floor’s surface free from slush and water and makes it easier to keep clean. The warm floor also helps to dry wet shoes and boots, making them lovely and warm to put on. In this the way, underfloor heating is an effective means of preventing a cold.
Product Choice for utility rooms
DEVIreg™ 130/530 or a timer thermostat DEVIreg™550 or 535 to adjust the temperature to your daily rhythm and, in that way, save energy. DEVIreg™ 535 includes a floor sensor, which will keep your floor warm regardless of the time of year.
DEVIlink for heating that is advanced, wireless, and easy to understand.
When renovating, we recommend using DEVImat™ DTIF or DEVImat™/DEVIflex™ DTIR to ensure a low height when installing floor heating on an existing floor.
For a new build, where the cables or mats are installed in the concrete slab, we recommend using DEVIflex™ DTIP, DEVIflex™ DTIE, DEVImat™ DTIP or DEVImat™ DTIE.