Byala Panorama Resort
The Byala Panorama Resort is situated in the charming town of Byala on some of the most beautiful coast line of the Black sea region in Bulgaria. The hotel is located just 350 meters from the beach and the local marina.
DEVI was chosen as a supplier of the floor heating solutions for all 111 hotel bathrooms. The installation was completed in 2007.
Project Overview:
Electrical floor heating
Project size: 111 bathrooms
Total output: 77 kW
Products:
DEVIflex™ DTIP 18
DEVIreg™ 530
Gallery
Project overview
111 bathrooms
Heating cables
Thermostats