National Bank Slovakia

Air transport is becoming more commonly used by private and business passengers. Helicopters are also more commonly used in emergency cases because of their features.

On May 23, 2002, the heliport on the National Bank of Slovakia building was opened. It is located on the roof, 110 m above the ground from Mýtna Street.

In order to provide safety for helicopters, regardless of any weather condition in 2000, DEVI electrical heating solutions were installed for melting ice and snow.

Project overview
  • 314 m2
  • Output: 76,2kW
Thermostats