NYX Hotel Warsaw, Poland

NYX Hotel is a spectacular complex with the tallest skyscraper in the European Union (310 meters high) grows right next to the Central Railway Station.
One of the smaller Varso office buildings will be the NYX hotel Leonardo network. The company has rented 20,000 m² of space. The facility will be ready in early 2020. It will be the first NYX hotel in Poland and the second is the Leonardo network. NYX is already operating in Prague and Milan. Hotels have compact rooms, free Wi-Fi. They are created in the centers of large cities. The Warsaw NYX will have 4 stars and 331 rooms that will take up to fifteen floors of one of the Varso tower. 331 rooms that will take up to fifteen floors of one of the Varso tower.
DEVIcomfort™ hating mats were used in all bathrooms in the NYX hotel. Interesting is that bathrooms were made as separate modules with Domczar company. DEVI heating mats were installed during assembly of each module in the Domczar factory and then transported into building site. This is a part of OEM cooperation that Danfoss has established with Domczar company. Domczar declares the annual module bathroom production of 8000 units. Large part of them will be equipped with DEVI heating mats.

Project Overview:

Project size:
662 m²
System output:
150 W/m²
Installed power:
99,3 kW
Year of implementation:
2019

Products:

  • DEVIcomfort™ 150T 2m² 331 pcs
Benefits Content Not Selected
Project overview

Project size:
662 m²
System output:
150 W/m²
Installed power:
99,3 kW
Year of implementation:
2019

Products:
DEVIcomfort™ 150T 2m² 331 pcs

DEVIcomfort