Shopping Arena, Austria
The shopping center Alpenstrasse was the first of its kind in the city of Salzburg. The visitors can now shop and eat in two houses on three levels on 23 500 square meters in 70 shops and restaurants. The two houses are connected by a wide corridor under the Alpine road. You can find many famous fashion brands are among the leading companies offering their goods and services on the shopping arena.
In 2014 DEVI was chosen to provide pipe protection for rain pipes.
Project Overview:
Purpose of the DEVI system: pipe tracing
Project size: 2100m
Installed power - total output 35,3 kW
Products used:
DEVIpipeguard – 10: 1200 m
DEVIpipeguard-25: 800 m
DEVIpipeguard-33: 100 m
Connecto AS – 73 pcs
Coccecto T – 13 pcs
Gallery
Project overview
- 2100 m
- Installed power - total output 35,3 kW
Heating Cables