Sun Village, Byala Black sea region
SUN Village Byala is a holiday complex with 18 houses. The beach of Byala with fine white sand, clean water is just 300 meter away the village. The SUN Village Byala is the only resort of its kind on the Bulgarian Black Sea coast. In 2007 the resort won an architectural award as the year's best project in the Varna region.
Also in 2007 DEVI floor heating systems installations for bathrooms and main rooms in 16 houses of the Sun Village was completed.
Project Overview:
Electrical floor heating
Project size: 16 houses
Total output: 52 kW
Products:
DEVIflex™ DTIP 18
DEVIreg™ 530, 535
Gallery
Project overview
16 houses
Heating cables
Thermostats