The National Azerbaijan Boxing Federation Office
Safety and comfort for boxers
During recent years, sport in Azerbaijan has become very popular, and the government is strongly supporting the development of sport centers. In 2014, the office of the National Azerbaijan Boxing Federation was constructed, and DEVI was chosen, not only as the electrical under‑floor heating solution, but also for the snow melting systems.
The building consists of two parts: one is the official entrance, lobby, office, and arena for the boxing fights, while the second part is a hotel for competitors and other guests. The installation of DEVI in the National Azerbaijan Boxing Federation was unique as almost all the various solutions offered by this brand were set up in one building.
Firstly, the DEVI snow melting system was installed in entrance stairs and on a large balcony. The system is automatically controlled by the DEVIreg thermostat. The next step was the installation of electrical heating in the lobby, entrance, and rest zones for guests. As electrical heating solutions are more and more often being chosen for saunas in the Caucasus and Central Asian regions, DEVI heating cables were installed in the saunas here too. The bathrooms in the hotel’s luxury rooms were also equipped with DEVI electrical heating cables.
The project was finished in May 2015. Now, the boxers and the guests can experience the comfort of DEVI’s reliable solutions.
Project Overview:
- Heating cables
- DEVIsnow™ 30T – 5,160 m
- DEVIflex™ 18T – 3,060 m
- Heating mats
- DEVImat™ 150T – 30 pcs
- Thermostats
- DEVIreg™ 130
- DEVIreg™ 850
NA