The Situla building, Ljubljana
DEVI solutions for ultra-modern design
The Situla building is a uniquely-designed construction complex, which extends over 80,000 m2 of overhead areas and has a variety of uses.
Underground parking
The 72-metre high residential tower contains 20 floors connected to the base by an 8-story tower extending along the entire building plot. A wide range of apartments was designed in the building: small single studios, medium-sized family apartments, duplexes, atrium apartments with patios, and also lofts.
The Situla contains 226 apartments, more than 6,000 m2 of office facilities surface, and more than 5,000 m2 of service establishments. The underground parking garage can hold 856 cars.
DEVI solution
Considering the comfort and safety of exploring the Situla building, DEVI was chosen to protect the roof, gutters and down pipes as well as the ground around the parking entrance. Thanks to simple and effective DEVI electric heating systems, the roof, the drain system, and the parking entrance of the Situla stays free of ice and snow during the winter.
Project Overview
- Pipe tracing
- 2,800 meters of pipe tracing
- DEVIpipeguard™ 10 self-limiting cable
- DEVIpipeguard™ 25 self-limiting cable
- DEVIreg™ 330 thermostats
- Roof, gutters & down pipes
- 1,500 meters of DEVIsnow™ 30T
- 3 x DEVIreg™ 850 thermostats
- 5 x roof sensors
- Ground area – parking entrance
- 1,130m² meters of DEVIsnow™ 30T
- 7 x DEVIreg™ 850
- 13 x ground sensors
NA