Reasons to install electric heating solutions for large public buildings
During its history, DEVI was chosen as the preferred supplier of electric heating for large public buildings, such as shopping malls, hotels, office buildings, and airports all over the world.
You don’t need to heat a whole volume of air in a 15 m high lobby, to be able to assure optimal thermal comfort for visitors (at 2 m height from flor level). Floor heating, ice & snow melting, pipe tracing and other applications are the core of electrical heating solutions offered by DEVI.
1. Experience with large construction
DEVI has proven co-operation with well-known shopping malls, hotels, offices, and other public buildings. DEVI is represented in over 66 countries and you can find public properties equipped with DEVI reliable solutions all over the world. Local DEVI sales companies provide large constructors with professional support and technical help to make our co-operation easy and efficient.
2. DEVI provides safety
Our solutions are chosen mainly to provide safety for driveways, walkways, roofs, and gutters as well as pipe tracing. DEVI’s ice and snow melting system is designed to provide safety for people, vehicles, and buildings through safe walking and driving, and less damage to buildings during winter.
Each centralized water system for public buildings, such as hospitals, hotels or multifamily blocks, should be protected against Legionella, not only via efficient filtration and disinfection but also by keeping water temperature within the control limits in the legionellosis risk. DEVI heating systems for domestic hot water meet demands of all required certificates for such pipe tracing.
3. Economical advantages
The DEVIreg™ thermostats with advanced moisture sensors (for outdoor systems) or opened window detectors (for indoor heating) ensure that optimal results are achieved with the least possible amount of energy.
It’s worth emphasizing that the costs of installing and running DEVI’s outdoor systems are low when the preventive advantages of the system are taken into consideration. You will easily avoid yearly investments in snow shovelling and salting. Furthermore, you avoid the repair costs caused by ice, snow, and salt damage.
DEVI has been chosen as the electric heating partner for buildings as hotels, shopping moles or rest homes, all over the world, mostly for budget reasons.
4. DEVI provides comfort
Floor heating is the most comfortable experience for guests of your hotel rooms or apartments. It distributes the heat evenly over the whole floor and provides appropriately pleasant warmth for your feet, body, and head. The wholesome heat surrounding your feet slowly rises and nicely warms your body. Underfloor heating makes it possible to lower the average room temperature by 2º C without affecting the degree of comfort. This means that the temperature can be reduced by around 20% - which is both an economic and an environmental advantage
5. Up to 20-year full warranty for DEVI cables and mats
All DEVI products are manufactured in the EU under the highest quality control. That’s why you can rely on DEVI. Due to the quality provided, we offer the best 20-year full warranty for DEVI heating elements, which includes costs of installation and floor materials, such as damage to brickwork and tiles.
Facts about Electric Heating by Danfoss Electric Heating by Danfoss is energy efficient and environmentally friendly meeting your needs in various applications. It enables you great comfort and convenience whilst ensuring user friendly solutions with lasting effect and highest quality standards.
Electric heating solutions are supported by legislations in key European countries. Directives that are coming in force in the biggest European markets give the green light to the trend: use eco-friendly systems and new materials ensuring energy saving.