BENEFITS
  • Cut to length on site
  • Ready-made lengths
  • Can be installed inside pipes

The DEVIpipeheat™ w/plug is a self-limiting heating cable that is mainly used for frost protection of pipes.

The self-limiting capability of the cable ensures that the output of the cable increase or decrease according to ambient temperature.

The heating cables can be installed on to the pipe system or inside the pipe as the cable is approved for use in drinking water. The DEVIpipeheat™ w/plug comes with an EU Schuko mains plug.